AOUT#.OFFSET

Description

This parameter sets the analog output offset.

Examples

Code

--> AOUT2.VALUEU 5
--> AOUT2.VALUE
5.000 V
--> AOUT2.OFFSET -1
--> AOUT2.VALUE
4.000 V
--> AOUT2.VALUEU
5.000 V

Context

For more information see Analog Output.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units V
Range -10V to +10V
Default Value 0 V
Data Type Float
See Also  
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen